Other Parts Discussed in Thread: UCC21520
Hello, I have identified the UCC27712 as a component which could satisfy my needs for a high-side driver, but wanted to confirm that I correctly interpret its specs.
I am using it to drive the SPW11N60C3 MOSFET, which has 300V coming from the power rail.
https://www.digikey.com/en/products/detail/rochester-electronics-llc/SPW11N60C3/12131755
I am not concerned about propagation delays in the system, but the critical factor is that I want fairly precise control over the actual "On-time" of the switch, which should be in the 25-40 nanosecond range.
The datasheet seems to indicate "minimum ON pulse that changes output state" that 25 nanoseconds is *normally* enough, with worst case being 45 nanoseconds. I don't know how likely or how often this "worst case" is to occur...but I wanted to just confirm that this would be an appropriate IC for my application?