This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ULN2803A: can we drive the input of ULN2803A using MCT6 with a forward current of 2 mA

Part Number: ULN2803A


Will this circuit work. Is the MCT6 output current sufficient to drive ULN2803 connected to a load of 200mA?