Other Parts Discussed in Thread: LM61495, LM61460
hello expert,
I am going to use LM61460-Q1 as CV_BUCK in my project, input is battery 9-20V,output is 4-7V,5A max,output load is LED drived by TPS92662.Pls surport the issue below
1.Pls check if the schematic is OK?Is there any suggestion,especially for EMC improvement?And is POWERGOOD signal no used in this case?

2.when Vin=9V and Vout=7V,the gap is small,will output undershoot happened when the output changed from light load to full load?This may cause flicker of the LED.And how to improve this issue?