This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22992SEVM: internal impedance

Part Number: TPS22992SEVM


Hi Team, 

I have a customer who reached out after testing this as they see that the actual measurements don't adhere to the Spec.

 

They have put a 5A load with Vin of 1.2V and Bias of 5V in 22 Celsius room temperature.

They have measured a voltage drop between the input and output of 70mV meaning that the internal impedance is 14mOhm as it should have been 8.7mOhm.

Could you please advise on this?

Thanks.

VL