Other Parts Discussed in Thread: TAS2552, , LM76002, , LM76005-Q1, LM76005
A small run (600) PCBA's with LM76003 as 3V3 rail from a 30..42 volt battery supply with a TAS2552 audio chip included. On quite a few (say 4%) of the boards, audio failed to start and failed MTE. Turns out the audio chip was just resetting due to a brown out of the 3V3. The audio chip would draw around 2.5 Amps normally.
- Schematic and SW/Freq pics included
- Static 2.5A load test results in rail being pulled down to 1.63V and staying there.
- RT resistor is normally unpopulated
- Bad board Fsw is ~750KHz
- Good board Fsw is ~500kHz
- All passives were removed and checked (except 4u7 inductor). No improvement.
- RT resistor changed from DNP to 82kohm and Fsw was now ~530kHz and SW waveform looked normal but CL issues persisted.
We have not reworked the LM73006 on the PCBA's (mainly because you can't lay your hands on TI parts these days) but visually and via xray, they look OK.
Any thoughts appreciated, I am thinking "IC start-up" since we have anecdotal evidence of the Audio starting correctly occasionally on some of the boards. But I have not seen this myself.LM76003_CL_Issue.zip