Other Parts Discussed in Thread: MSP-EXP432E401Y,
The user’s guide of the BOOST-LP5569EVM mention the MSP-EXP432P401R but is no more in production, in fact the link in the PDF is directing to the new MSP-EXP432E401Y, but I’m not able to execute the LP5569EVM_GUI on this new MSP-EXP432E401Y.
When the application start, a message ask for:
Firmware Vesion : F.1.0.7 is required.
but the update of the FW does not work. I receive the following error:
DSLite version 6.2.1.1595
Configuring Debugger (may take a few minutes on first launch)...
Initializing Register Database...
Initializing: CS_DAP_0
Executing Startup Scripts: CS_DAP_0
Initializing: CORTEX_M4_0
Executing Startup Scripts: CORTEX_M4_0
Connecting...
fatal: CS_DAP_0: Error connecting to the target: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the ReadMe.txt file there for instructions. (Emulation package 6.0.222.0)
Could you help me?
Thanks