Looking through the TPS65951 datasheet, I see references to bluetooth PCM and timing diagrams, but I thought one of the things that separated the TPS65950 and TPS65951 was the lack of bluetooth PCM interface. Ball C3 is even listed as BT.PCM.VDR. Is this a typo?
I am working on a design using an AM3703 in CUS package and was considering the TPS65950, but I would like to avoid the 0.4mm ball spacing. I am also going to have a PAN1315 bluetooth radio module on board and was going to use the bluetooth PCM interface on the TPS65950. What would be my best option for the bluetooth PCM if I were to use the TPS65951?
Thanks