This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL4242 VIN and PWM tied together

Other Parts Discussed in Thread: TL4242

Is it an acceptable use of this device to tie the PWM & Supply input pin (I) together to receive a PWM input signal (24V or 35 V; 200 Hz) for varying the output LED power.

What considerations should be thought of?

  • Ed,

    We have taken data with the TL4242 EVM with I and PWM pulsing from 0V to 12V through 40V and duty cycles from 10% to 100% (200Hz) and see no issues at all.

    A summary of the data will be posted upon complete analysis.

    Considerations should be Thermal dissipation at the high duty cycle end along with power up / down timing at the low duty cycle end.

    Regards,

    Dick