Part Number: LM5146
Hi Team,
Do we have constant current control scheme based on LM5146 to recommend? Customer is consulting about it. Thanks.
Best,
Stanley
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5146
Hi Team,
Do we have constant current control scheme based on LM5146 to recommend? Customer is consulting about it. Thanks.
Best,
Stanley
Hi Stanley,
See appnote below on implementing an CC/CV converter.
https://www.ti.com/lit/an/snva829/snva829.pdf
You will have to use a circuit like figure 1 with an external current sense amplifier that injects onto FB node.
The design equations are also in the figure.
Hope this helps,
-Orlando
Hi Orlando,
Thanks for help. What if customer want to control the COMP pin of LM5146 to achieve CC(pull-up or pull-down during 0~5V range), what's the risks they may encounter? Do you recommend to do that?
BTW, do you have more detailed schematic based on figure 1 of snva829 here? Customer has no experiences in it.

Best,
Stanley
Hi Stanley,
Why do they want to inject into COMP instead of FB?
I don't recommend actively controlling COMP voltage, COMP is powered internally by the error amplifier and also has internal clamps that could be susceptible to damage.
Also COMP dynamically responds to load transients in the CV condition, I wouldnt recommend messing with the COMP response.
We suggest you inject into the loop at a high-impedance node like FB.
Hope this helps,
-Orlando