Other Parts Discussed in Thread: LM5143-Q1
Hi team
Could you help check if LM5145 is a good option for the 12V to 0.85V/35A application?
WEBENCH shows its maximum load current is only 20A, and the product folder shows its maximum load current is 30A, and both are smaller than the 35A requirements