This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62745: TPS62745 failed to regulate at super low load-10mA

Part Number: TPS62745


Hi Team,

I am using the TPS62745 regulator and have the input ~ 8.7V and output voltage set  to 3.3V. The output is regulated at beginning without load, however when the 10mA load  is connected out voltage is dropping to 0.V, it seems to fail the regulation with lower load,Can I have some help to understand why this is happening please?