This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS70618DRVR is powered by 3.3V regulator(LDO) and the output is connected to VOC(volatile organic compounds) sensor IC which works on the minimum voltage of 1.68V and nominal voltage of 1.8V. the enable pin of the TPS70618DRVR is connected to output pin of the microcontroller(powered by 3.3V). but if we observe the voltage of the output of LDO and the Enable pin we found that there is a some glitch in the enable signal and the output of 1.8V (refer the below picture). the Problem we are facing is we are not able to read the VOC data which is powered by this 1.8V. This issue we are facing with the TPS70618DRVR part but with the TPS78218DRVT it works fine.
CH1.--1.8V OUTPUT CH2:-ENABLE
Hello Sumeet,
Are all 4 images the same scenario? Also, is it possible to share the schematics of the circuit including how TPS706 is powered? Lastly, is there a way to apply a voltage to Ven without the Microcontroller?
Best,
Edgar Acosta
Hello Edgar,
3.Yes, applied the voltage to Ven pin there is not glitch observed , but what is the reason when we connect this to the microcontroller it shows the drop.
Thanks,
Sumeet P.
Hello Edgar,
Can you please update on this.. is info provided sufficient or do you need more information on this??
Hi Summeet,
I apologize for the delayed response I was OoO.
Thank you for sharing this information.
Is the MCU powered through the same rail as TPS706?
Is there a way to test the 3.3V from the MCU without the LDO? There is an internal pull up resistor between Vin and Ven, therefore, EN can be left floating and still enable the device:
I suspect it might be the current needed for the EN pin and/or the interaction of the MCU with the LDO:
As for TPS782 the Ien is lower and does not have the same EN internal circuitry, therefore, the glitch does not exist.
Best,
Edgar Acosta