This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55288: Can I use TPS55288 as TEC driver?

Part Number: TPS55288

Dear team, 

I would like to use TPS55288 as a TEC driver using VIN-VOUT difference like below concept. 

Can I use TPS55288 as a TEC driver? Please review below concept and let me know your opinion. 

- 6V input / 1V output , Vin - Vout = 5V, current : 0.6A 

- 6V input / 11V output , Vin - Vout = -5V, current : -0.6A

- output voltage control : I2C

Thank you