This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2663: TPS2663 Model not native in PSPICE for TI

Part Number: TPS2663

Hi There

I try to build a simulation with the TPS2663 with PSPICE for TI. 

The model is currently not in the native TI library built into the software. 

Because of that i get the annoying promt that i can only use between 1 and 3 markers. This is quite annoying, especially when the part is actually a TI part. 

Is there a possbility to add the model to the library?

Thanks and best regards,

Jonas