Hi,
I'm using the TPS7H4010-SEP in a new design.
We are at the stage of architecture, and studying the effect of single point of failure of the component.
If we consider a failure of High side or Low side transistor (for exemple in short circuit), can we consider the PGOOD is immune to propagation and remain functionnal ? Maybe the function is segregated on the chip?
Do you have any data or recommandation for this case to study ?
The main idea is to use the detection (by PGOOD state) of an Over voltage or Undervoltage on the output in case of failure to passivate it.
Thankyou in advance for your help
Best regards
Jean-Irénée Hullo
Power & Analog Designer