This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25184: 12V to 8~9V/2A application

Part Number: LM25184
Other Parts Discussed in Thread: LMR36520

Hi team

My customer is designing an isolated power board: 

  • Vin=12V 
  • Outpuut=8~9V/2A

Could you help check if LM25184 is a good option for this application? Do you have other recommendations? 

  • Hello Shawn,

    With the team's offerings available, a flybuck solution potentially maybe a good fit.

    IE:LMR36520

    AppnoteI

    The flyback solutions we have available have two low of sw current limit and would require too high of a turns ratio, which would exceed the absmax on SW.

    The flybuck solution could enable the customer power condition at a consequence of poorer line and load reguation, and also, potentially efficiency.