Hello!
On what chip would you recommend building 48v phantom power for condenser microphones?
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Input voltage 12V-15V from battery.
The output current is minimal. I don't know how small it is. I think about 50-100 mA.
There are many chips like TPS61170. I would like to know the best solution for sound recording equipment. With minimal ripple and noise. Quality in this case is more important than price.
Hi Gennadiy,
Do you need the output converter output 48V DC voltage? TPS61170 Vout is only up to 38V.
Hi Gennadiy,
You can consider using LM5158, the 85V output boost converter.
Thank you!
Unfortunately, the LM5158 chip is not currently on sale either in Lcsc or even in Mouser. Though Lcsc is preferable. I order printed circuit boards and assembly from them. If you buy in other stores, you will have to install the chip manually. In this case, it is highly desirable that it be available in a DIP package.