Hi Team,
Our customer is looking for assistance in designing an isolated buck-boost converter with COTS transformer. According to our customer, all attempts to use the TI WEBENCH Power Designer results in a design requiring a custom transformer. They were hoping TI had done a similar exercise in the past or for another customer that resulted in a COTS transformer being used. Below are the power supply specifications.
Input voltage: 20-40V (45V tolerant is preferred but other protection can be added if needed)
Output: 30V @ 2-3A
Temp Range: -40C to +85C min
Regards,
Danilo