This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

A gate driver for high side N-mosfet

Other Parts Discussed in Thread: TPS4811-Q1

Hi,

I want to put an N mosfet in high side of the load connection point for protection purpose, it is not for PWM, just work as an on off switch, when a short circuit in the load is detected, it opens. The high side bus voltage is 65V. Is there a simple solution for the gate driver, that doesn't need isolated power supply?