Other Parts Discussed in Thread: TLVM13640, TPSM63602
Hi support team,
Is TLVM136x0 a low cost version of TPSM6360x?
Are these differences below?
| TPSM6360x | TPSM6360xS | TPSM6360xE | TLVM136x0 | |
| VOUT range | 1 to 16V | 1 to 16V | 1 to 16V | 1 to 6V |
| External clock synchronization | Yes | Yes | Yes | No |
| Adjustable Switch-Node Slew Rate (RBOOT and CBOOT) | Yes | Yes | Yes |
No (TLVM13620/30) Yes (TLVM13640/60) |
| Spread Spectrum | No | Yes | Yes | No |
| Extended Temperature Range | No | No | Yes | No |
Please let me know if there are any other differences.
Regards,
Dice-K