Other Parts Discussed in Thread: BQ25792, , TPS25750
Hi Team,
I understand that IINDPM(ILIM_HIZ)=500mA setting on EVM and don’t connect D+ and D- pins.
Currently, our customer can provide output current 2.5A at the following conditions.
So, input current limit is more than 500mA.
<Conditions>
VBUS=20V/2.25A (45W)
VSYS=16V
IOUT=2.5A
<EVM>
I have two questions.
--------
[Q1]
Could you please let us know the input current limit value of BQ25792 on EVM?
[Q2]
How long is " IINDPM(ILIM_HIZ)=500mA " applied after startup?
By the way, I found “9.3.4.5 Input Source Type Detection” and “9.3.4.5.1 D+/D– Detection Sets Input Current Limit” in datasheet.
D+ and D- pins of are open on EVM so I guess that BQ25792 can’t detect D+ and D-.
Therefore, BQ25792 don't know the timing of " 1. Input Current Limit (IINDPM) register is changed to set current limit".
--------
Regards,
Hide