Hi
Query-1:
We plan to use MPN # TPS65023QRHARQ1 to connect with i.mx6ULL nxp's processor. We have gone through the pin assignment and have a query with pin#27 "RESPWRON".
Can we connect this pin to the i.mx6ULL POR pin(P8)? As per the i.mx it's Power on reset functionality in the SNVS domain and has an internal Pull-up.
Query-2:
i.mx pin(T9) "PMIC_ON_REQ" is connected to which pin of PMIC?
Appreciate in advance.