Hi I've reviewed the information in the DataSheet and done the calculations myself
I've included the xls file with all the formulas, the tabs are labeled accordingly to the component that is being evaluated
If you need to find any label just look under "Insert/Names/Define" or check the properties for the file.
I need some help here verifying that I will not end up with a 0% efficiency supply.
My biggest concern is that the units appear to be mixed in the formulas given in the data sheet, if I enter the units in the formulas, values don't add up in some, but they appear to add up in others.
Any feedback and help is greatly appreciated
Thank you.
Regards.4477.Calculations.xls