Other Parts Discussed in Thread: TPS62810-Q1
Hello team,
I want to double check if TPS62816-Q1(6A) is p2p compatible with TPS62810-Q1(4A). And is it oaky to use the same schematic as TPS62810-Q1?
Thanks,
Sam Lee
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team,
I want to double check if TPS62816-Q1(6A) is p2p compatible with TPS62810-Q1(4A). And is it oaky to use the same schematic as TPS62810-Q1?
Thanks,
Sam Lee
Hi Sam,
Thanks for your question.
The devices are p2p, but if you refer to the Recommended Operating Conditions you will see that the inductor / output capacitors ranges are different for the two devices.
Therefore you should properly tune the BOM when changing device.
Thanks,
Stefano