This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256303: Webench Design of LLC Circuit

Part Number: UCC256303

Hi Team,

Our customer simulated the UCC256303 in Webench and before he build the board he would like to ask for your opinion if the design will work. 

https://webench.ti.com/power-designer/switching-regulator/export/158

Additionally, he would like to clarify about the custom parts mentioned in the BOM. It seems that these parts are not readily available from distributors, does he really need an ESR of 1 mΩ? If not, what is the lowest ESR of readily available parts he can use?

Cin CUSTOM CUSTOM 1 0 Cap: 47 µF Total Derated Cap: 47 µF VDC: 100.8 V ESR: 1 mΩ Package: null
Cinx CUSTOM CUSTOM 1 0 Cap: 1.5 µF Total Derated Cap: 1.5 µF VDC: 92.4 V ESR: 0 Ω Package: null
Cr1 CUSTOM CUSTOM 1 0 Cap: 304.29 nF Total Derated Cap: 300 nF VDC: 85.21 V ESR: 1 mΩ Package: null
Cr2 CUSTOM CUSTOM 1 0 Cap: 304.29 nF Total Derated Cap: 300 nF VDC: 85.21 V ESR: 1 mΩ Package: null

Regards,

Danilo