This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EV2400: Not detecting with Windows 11?

Part Number: EV2400
Other Parts Discussed in Thread: BQSTUDIO,

So I have EVT2400 which was working fine for me couple of months back, then I needed to check something again with BQStudio but now it's not getting detected. I tried to search on this forum to see what I can do. LEDs are on, I have tried updating the FW and it was updated without any error. When I connect with my laptop I can hear the USB connection sound but it doesn't show any notification or anything in device manager. I have made sure all my USB drivers are up-to-date. For once just for one time it showed in device manager with yellow exclamation mark " “Unknown USB Device Descriptor Request Failed” but it never showed again in device manager nor it's getting detected by BQStudio. I also tried it with Windows 10 as well as previously I was using it on Windows 10 but it's not getting detected there as well.