Hi Team,
Need your assistance on this. I'm trying to control the Discharge FET by using the DFETOFF pin. However, this feature disable completely any protection feature of the FET, such as the body diode protection in charge. As a result, when the battery is charging, there is a lot of power loss, since my DSG FET is not enabled for body diode protection.
Is there a method to implement FET control without an external MCU, but including such body diode protection?
I tried a workaround, setting the DFETOFF pin as cell thermistor and enabling the Over Temperature Discharge protection. It seems to work well, however the protection release is too slow, and the battery turns on with 5s of delay approximately (also with Protections:Recovery:Time = 0s).
Kind Regards,
Jejomar