This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50: the verification of the device.

Part Number: BQ40Z50-R4

I have read data via 0x44 ManufacturerBlockAccess() like the following examples.

Command (Function) : Value
0x0001 (Device Type) : 00 45
0x0002 (Firmware Version) : 45 00 04 02 00 4F 04 04 75 02 00

But I don't know if the values are correct.
I don't know Device Type, Device Numver, Version, Build Number, Firmware Type, Impedance Track Version.
How can I know what they are?

Can you recommend how to check if the values are correct or not?

 

And, on Datesheet, it says "if Data read = 06 00 00 01 (each data entity is returned in little endian), the command is 00 06 and the value is 01 00."
So it says "The value is 100."

Ok, I understood that.

So, for 2 bytes data like 0x0057 (ManufacturingStatus),
if Data read = 57 00 78 00,
the value would be 00 78.

But what about 4 bytes data like 0x0051 (SafetyStatus)?
If Data read = 51 00 12 34 56 78,
what is the value?

Thanks.