Part Number: TPS780
Other Parts Discussed in Thread: TPS62840, , TPS7A94, TPS7A02, TPS7A57, TPS7A85A, TPS7A84A, TPS7A83A
Hi LDO folk,
There would be three types of LDO devices ; fixed output, adjustable output, VSET type output. I wonder if TI has device with VSET type like TPS62840. TPS62840 has internal resistor to digital converter to determine the output voltage by only one resistor. Customer wants to reduce FB resistors in LDO.
TPS62840 1.8-V to 6.5-V, 750-mA, 60-nA IQ Step-Down Converter datasheet (Rev. D) (ti.com)

Question 1.
I notice TPS780 has internal EPROM to control the output voltage level. But this device is applicant only for a specific MCU application and its current rating is too low for my customer. Do we have another LDO device with VSET pin and the higher current rating?
Question 2.
Customer has a concern on internal EPROM because it will be clocking and it can be an noise source in system level. Can you share your thought on this concern?
Question 3.
Due to the concern in Question 2, customer prefers integrated ADC like TPS62840. Do we have this type of LDO?
Thank you!