Other Parts Discussed in Thread: BUF602, , LM3671, CC2650, FDC2214
Dear TI experts,
Can the ±5V output of TPS65133 supply power to BUF602 a high speed unit gain buffer?
Sorry, this question might be too basic. According to the datasheet, ±5V is exactly what the BUF602 needs.
But I still want to confirm if this design is feasible.
Also, I have a question about powering the TPS65133.
Can I use the output of the DC-DC converter LM3671MF-3.3 (Vout 3.3V, Ioutmax 600mA) to power the TPS65133?
Or directly use a 3.7V lithium polymer battery for power supply, which is better in efficiency and power consumption?
One last question about AGND and PGND in the layout.
Can I simply use a single GND in the schematic and PCB layout?
Best regards,
Will