Part Number: TPS51124
Hi Team,
A Japanese customer has a inquiry on how to select pull up resistor on PG pins.
Can I get your valuable suggestion?
He want to know the relationship between the pull-up resistance value of PGOOD1 and 2 of TPS51124 and the IPGMAX current value.
Q1: Since the current value of IPGMAX is MIN2.5mA, should I set the PGOODx pull-up resistance value to 1.2kΩ for 3V voltage?
Q2: When PGOODx pull-up resistance value is set to 10kΩ Is the current value of IPGMAX about 0.3mA at 3V voltage?
IPGmax is Min 2.5mA, typ. 5.0mA in the datasheet.
Customer is anxiously waiting for this reply, I appreciate for your quick response.
Thanks.
Regards,
Frank