This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25942A: Basics of eFuses (SLVA862A)

Part Number: TPS25942A
Other Parts Discussed in Thread: TPS25947

Hi All,

I have a question about the eFuse application report Basics of eFuses (SLVA862A).

What is the difference between "Reverse Current Protection" and "Input Reverse Polarity Protection" in the protection function of eFuse?


Best Regards,
Ishiwata

  • Hi Ishiwata,

    Thanks for reaching out.

    1. Reverse current protection means blocking reverse current . For eg suppose VOUT>VIN, then reverse current can flow if protection is not there.

    2. Reverse polarity protection means protecting the load and device when input voltage polarity is reversed for eg connecting reverse battery.

    Regards

    Kunal Goel

  • Hi Kuna,

    Thank you for your answer.

    Comparing the TPS25942A and TPS26600, I think they have the same structure because they have a NMOS and an PMOS.

    Does the TPS25942A have an "Input Reverse Polarity Protection" feature?
    Does TPS26600 have a "Reverse Current Protection" function?

    I am very grateful for your support.

    Best Regards,
    Ishiwata

  • Hi Ishiwata,

    Yes they have similar structure. Both are NMOS in back to back configuration.

    1. TPS25942 does not have inbuilt IRPP. You can use external diode like this to achieve IRPP. TPS25947 has inbuilt IRPP and RCB.

    2. TPS26600 has both IRPP and RCB.

    Regards

    Kunal Goel

  • Hi Kunal,

    Sorry for my late reply.

    I understand the difference between them.

    I am very grateful for your support.

    Best Regards,
    Ishiwata