Other Parts Discussed in Thread: EV2400, BQSTUDIO, BQ25798
I have my BQ25798EVM hooked up with a BQ34z1xxEVM and an EV2400 in the following test setup...
When cable m15 is connected, the bqStudio goes straight to the BQ34z1xxEVM screen. But when I want to use bqstudio for the BQ25798EVM, I have to disconnect m15. Then bqstudio gives me a "Supported Targets" screen where I can select between Gauges, Chargers, etc. After I select Charger > Charger_2_00-bq25798.bqz, I sometimes get the correct screens for running the bq25798; sometimes I get an error message that says "No free adapters are available for use on this system."
It's inconsistent and is making my evaluation more difficult.
How can I move back and forth from within bqstudio to target either the gauge or the charger?
Carl