Other Parts Discussed in Thread: BQ25300, BQ34Z100-G1, BQ27Z746
Hello
I am Developing IIoT device that runs on 12000mAh LiFePO4 battery. I am trying to find an energy efficient Battery Charger with Power Path to be utilized in the design. BQ25300 is a nice chip but it's not available in stock anywhere. The best option I was able to find is BQ25181, which can simplify my design but the charging current is limited to 1A. I would like to ask couple questions before I integrate the chip into the design...
The initial design architecture was based on BQ25300. Since the output is not regulated, a DC-DC boost converter was used as shown in the image below.
The updated architecture is based on BQ25181. The boost converter was removed since BQ25181 provides regulated output.
1) Please let me know if you agree with the new architecture.
2) BQ25181 Datasheet indicates "system loads of up to 2.5 A". The IIOT device will have <1A average current with a burst current up to 2A. Is that within the capability of the chip?
3) Given all different charging modes the chip will cycle though, how long does it take to fully charge 10Ah battery?
4) Any suggestion for LiFePO4 battery gauge?
Thank you