Other Parts Discussed in Thread: TPS61288
I required 12V/2.2A Output from 5V input what can i need changes in Schematic
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Vishal,
The input current is calculated as (12V*2.2A)/(5V*0.8)=6.6A when assuming efficiency is 0.8. The switch current limit needs to be more than 7A at least. So LM2623 doesn't satisfy your requirement.
For your application, TPS61288 is recommended. The 5Vin to 12Vout/2A schematic is as followed.
Regards,
Bryce
Hi Vishal,
You can access TPS61288 on the product page. Click "Add to chart" or buy it from distributors.
Bryce