Other Parts Discussed in Thread: BQ25798, , BQSTUDIO, EV2400
I am trying to harvest power from a solar panel into my bq25798 charger.
I have the solar panel connected to the J1 port of the BQ25798EVM. With no light the Vin is low and the battery discharges into my 419mA system load. When I illuminate the panel I get 7.98V at Vin, but no current. The battery pack continues to discharge into the load.
Then, when I switch from the Solar Panel to a bench supply at J1, set to 7.9V and current limit to 2.5A, I get the expected results: the power supply feeds the load and also gives a little charge current to the battery pack. What do I need to do to get my Solar Panel to behave like my power supply? Is there some setup needed on the BQ25798EVM?
Please let me know. Thanks,
Carl