Hi team,
my customer is doing schematic with TPS61089 please help review this and give feedback. Add one question, can this part support MLCC+POSCAP?
thanks and best regards,
SophiaAMP TI.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
my customer is doing schematic with TPS61089 please help review this and give feedback. Add one question, can this part support MLCC+POSCAP?
thanks and best regards,
SophiaAMP TI.pdf
Hi Eric,
customer use 61089 provide power for two smart amps, RMS 320mA peak 1300mA for one amp and two amps load current will double(RMS 640mA peak 2600mA). And Vin is 6.5V~9V. Customer said that they can avoid MLCC noise issue in light load by using POSCAP.
一个amp RMS 320mA peak 1300mA
我们是2个amp 所以 RMS 640Ma peak 2600Ma
Vin range 6.5V~9V
使用POSCAP是为了避免或者降低轻载时候MLCC 产生的啸叫问题
PVDDH(10V) |
0.1uA |
(2W 平均电流) 320mA RMS |
1300mA peak |
Hi Sophia,
The sch is basically okay. COMP parameter can be optimized. Rcomp (PR1510) is recommended to change to ~15k, Ccomp (PC3978) changed to 4.7nF. Cff (PC3979) changed to 10pF.
Typically, we don't use POSCAP. Customer can use several small value MLCC or add one electrolytic capacitor.
Best Regrds,
Eric Yue