This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1A: Can BQ78350-R1A work together BQ79616 ? and is there a reference circuit ?

Part Number: BQ78350-R1A
Other Parts Discussed in Thread: BQ79616, , BQ76920, BQ76930, BQ76940, TIDA-010030, BQ34110, BQ34Z100-G1

Hi 

Can BQ78350-R1A work together BQ79616 ? and is there a reference circuit ?

  • Hi PY, 

    The BQ78350-R1A can only work together with the BQ769x0 battery monitor family (BQ76920, BQ76930, BQ76940). 

    The BQ34Z100-G1 and BQ34110 are more flexible and can work with other battery monitors since these gauges are independent from the monitor. The TI Reference Design TIDA-010030 shows an example of using the BQ34Z100-G1 with the BQ76940.

    Best regards,

    Matt