This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR51420: How to calculate power dissipation of LMR51420

Part Number: LMR51420


Hi,

For one of my battery operated application board i am planning to use the LMR51420.  specifications are ;

input voltage :4.75 V to 20V 

Output Voltage : 4V

Output current : 1A

Max operating temperature : 60 degree C.

As i have calculated

Pd = (Tj-TA)/RθJA , which is Pd = (125-60)/107.8 = 0.629 W. 

and 

Actual power dissipation = I2 Rds(on) = 1ˆ2 * (0.12 + 0.07) = 0.19W.

It looks fine per my calculation.

please suggest.