Other Parts Discussed in Thread: BQ40Z50, BQSTUDIO
Hi,
can you please let me know how can I enable VOUT1 3.3V output on EV2400, I would like to use it to power external electronics.
Regards,
Jun
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jun,
Vout can be set to 0V or 5V only.
To control this pin, Start bqStudio and select any bq40z50 device. Then click on "Registers" tab. Go to menu "Autocycle" and use the "2 pin control" "Enable load" to change the status. Checkbox next to that menu means it is set to 5V, otherwise it is set to 0V