Hello. Please offer clarity on when ACDRV is enabled on the BQ24780s.
From the datasheet, the ACDRV is dependent on CMSRC. Yet CMSRC follows after the ACFET is enabled. Respectively, see this as a paradox on how can ACDRV be ACIN+6v for the gate of the ACFET when the ACFET is not yet ON ?
One thread on this forum mentioned that the REGN (6 volts) is used at the start of this enable cycle of ACDRV but again, if we have 19v on the input of the ACFET, we require 19+6v = ~25v on gate to enable this first fet.
VCC = 19v.
ACDET is > 2v4.
ACOK is typically pulled up to REGN.
What are we missing in our understanding ?
Also, is REGN a fixed ON LDO or will it turn OFF under some condition inside the BQ24780s ?
Thanks!