Other Parts Discussed in Thread: TLVM13620, LMR43610
Please find attached schematics.
Vin = 10V to 30V
Vout = 5V
Iout = 50mA to 100m



During 5V turn-on high inrush is observed. I am using a 1uF capacitor on the SS pin which is the maximum recommended per the datasheet.
Do you think the inductor value should be high to support the light load and avoid this inrush? Does small inductor value cause this issue?