Other Parts Discussed in Thread: TPS62A01, TPS62A01A
Hello,
customer needs min value for the power good threshold. We only listed typ values. For worse-case scenario he needs the min to have a defined reset for the processor.
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Holger,
As TLV62568A is a cost optimal solution, we only have characterization data for it at typical conditions. If the customer needs to get data at worst case scenarios, then they might use an alternative device which has been characterized for corner cases as well.
TPS62A01/TPS6201A is a possible alternative which is also cost comparable to TLVs.
Here is the link to the datasheet:
Thanks!
Best regards
Sneha
Hello Sneha,
there are also no min/max power good threshold for the TPS62A01/TPS6201A.
Regards, Holger
Hello Holger,
I apologize I missed it.
I checked the data internally for TPS62A01/TPS62A01A. Here are the values:
1) PG Low, FB Falling: Min Value = 92.1 %, Max Value = 94.5%
2) PG High, FB Rising: Min Value = 94.8%, Max Value = 97%
Thanks!
Best regards
Sneha