Other Parts Discussed in Thread: LP5861
I understand that LP5018 is a RGB led driver, with brightness bank control for 3 led outputs. As per datasheet, there are only below registers available for controlling led brightness through PWM( 3 bank channels, 6 individual leds). Refer below image.
I would want to glow 15 leds(single color) individually at a time or all together using PWM. Is this possible by using OUTx_Color registers (0Fh~20h) if the color of the leds are fixed? if yes, how the same can be done? is there any equivalent alternate with similar specs for glowing single color led( constant current with low iq/enable pin) with 15 channel.