This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The load transient form no load to full load at 100 kHz will be required in most of applications, even some applications require higher frequency, so this test is ok.
Do you look at the output current/voltage waveform, which cause the failure?
And measure the Bode plot of control loop to check if the control loop is designed well?
Regards,
Teng
Hi Teng,
Replying to --> The load transient form no load to full load at 100 kHz will be required in most of applications, even some applications require higher frequency, so this test is ok..
May i please know in which application, load will be toggled from no load to full load at 100 kHz
Hi,
It is a generate test item for power module.
please measure the Bode plot of control loop to check if the control loop is designed well?
Thanks,
Teng