Hi
I have 2 BQ24005 damaged after I power up the PCB.
R2=11.5k and R3=40K (my thermistor is a 10K).
After burning the first sample I populated a second board and I powered it up without the battery connected. I observed a very low power consumption and the timeout (pre-charge) correctly. Then I inserted the battery and the LED D2 light up and the current observed matched the one expected (aprox 1A).
Then I power down everything and with the battery inserted I power up the circuit again. From that moment on the second BQ24005 got burn also.
Any idea/ advice?
Thanks
Joao Martins