Other Parts Discussed in Thread: LM5160
-
Customer use LM5160A need compatible with 24V/5V inputs to meet the end customer voltage.
- When they use 24V Vin,the LM5160 can work well;but when the Vin is 5V,they do not need LM5160A work,5V Vin connect the Diodes cathode of LM5160A'S Vout(Can find below picture) .BTW,no matter what Vin is 24V or 5V,the LM5160A is in the PCBA.They want to know if the LM5160A can work like this way?