Hi,
After reading different posts from this forum relating to some PWM managment issues with the CTRL pin when the voltage on the CTRL pin is set to 3.3, 5V, managed by an Arduino or not , I encountered the same kind of error.
Following the type of the interface (value of the pull-up, value of the reference voltage of the pull-up, direct management by a logic gate) the PWM works fine or not. The timings of the PWM don't change between the tests [and the 160µs low state is always respected without any glitches below 50 ns).
Although I notice that the current flowing into this CTRL pin is quit high (7 mA for a +5V logic gate with a Vin at 12v) and if I don't have a certain amount of current (let say 2/3 mA) I encounter some issue (no backlight on or a PWM management).
Do we need a specific amount of current into this PIN during the PWM mode (without easyscan)? Is it normal to have around 7 mA flowing into this pin ?
Picture attached is the current into the CTRL pin from my logic gate (only the timing and Ipp are relevant)