We're trying to use a BQ25180 to charge a LiFePO4 cell, but it's not working. The BQ25180 doesn't indicate any faults, though. Here's a register dump:
0x0 (STAT0) -- 0x01 (should be 0x41 if it were charging)
0x1 (STAT1) -- 0x00
0x2 (FLAG0) -- 0x00
0x3 (VBAT_CTRL) -- 0x0A (3.60 V is the target)
0x4 (ICHG_CTRL) -- 0x2A (charging enabled, 150 mA fast-charge current)
0x5 (CHARGECTRL0) -- 0x1C
0x6 (CHARGECTRL1) -- 0xE7
0x7 (IC_CTRL) -- 0xC7
0x8 (TMR_ILIM) -- 0x4D
0x9 (SHIP_RST) -- 0x11
0xA (SYS_REG) -- 0xE9
0xB (TS_CONTROL) -- 0xC8
0xC (MASK_ID) -- 0xF0
Measured battery is 3.25 V, and TS is at 0.39 V, which looks to me to be safely in the normal range. Input power is 5 VDC through a Schottky diode (not shown). We are not using SYS. We are not planning to use the Wake timers nor Ship Mode.
What are we missing?
Thanks,
Scott