This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS75003: When not using buck controller 2 and minimum load current

Part Number: TPS75003

Hi All,

I have a question about TPS75003.

(1) Is there a minimum load current value for back controllers 1 and 2?
      If so, please tell me the value.

(2)If not use buck controller 2,How should I connect each pin?
 I think that it is as follows.
   VIN2:GND
   SW2:Open
   EN2:GND
   FB2:GND
   SS2:GND
   IS2:GND

Is this correct?


Best Regards,
Ishiwata